You are here: Describing KAS Graphical User Interface > Windows and Panels Overview > Information and Logs > Compiler Output

Compiler Output

Compiler Output

Figure 3-15: Compiler Output

This tab displays information about the last project compilation. It shows information messages as well as Warnings and Errors (highlighted in red). Successful and unsuccessful output is reported within this tab to help identify and troubleshoot problem areas of the program development.

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™