You are here: Describing KAS Graphical User Interface > Windows and Panels Overview > Dictionary > Structures

Structures

All the structures within the entire system project are grouped as follows:

Structure

Description

EtherCATCode

List all the devices as PLC"Programmable Logic Controller" A Programmable Logic Controller, PLC, or Programmable Controller is a digital computer used for automation of industrial processes, such as control of machinery on factory assembly lines. Used to synchronize the flow of inputs from (physical) sensors and events with the flow of outputs to actuators and events variables so you can use their names in FBs instance

PNCode

List all the variables related to the specific Pipe Network Code

ProfilesCode

List all the variables related to the specific profiles

PLCopenCode

List all the variables related to the specific PLCopenA vendor -and product- independent worldwide association active in Industrial Control and aiming at standardizing PLC file formats based on XML Code

UDFB"User Defined Function Block" UDFB can be used as a sub-function block in another program of the application. It is described using FBD, LD, ST or IL language. Input / output parameters of a UDFB (as well as private variables) are declared in the variable editor as local variables of the UDFB variables

List the variables related to a specific UDFB

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™