You are here: KAS IDE Reference > Menus and Toolbar Overview > Main Toolbar

Toolbar

The main toolbar of the KAS IDE"Integrated development environment" An integrated development environment is a type of computer software that assists computer programmers in developing software. IDEs normally consist of a source code editor, a compiler and/or interpreter, build-automation tools, and a debugger (Tools) contains the following icons:

Icon

Description

Create a new project

Open an existing project

Save the project

Print the project item currently open in the workspace

For more details, refer to Print

Print preview

Undo

Redo

Cut

Copy

Paste

Find

Toggle Edit/Debug mode (enabled when the application is running)

For more details, refer to PLC Online Change

Table 4-8: Main Toolbar Icons

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™