You are here: Advanced Topics > Coordinated Motion > Overview > Coordinate Systems

Coordinate Systems

There are three different coordinate system (CS) types:

Figure 11-1: Examples of CS types on a machine and part.

Many coordinated moves may be done in a choice of coordinate systems. The differences between the types are offsets and possibly transformational algorithms to convert between the different systems, which ultimately control the actual axes on a piece of machinery.

For example, the X-axis of a Machine CS is meant to command a pair of Axes CS axes (X1 and X2) which together form a gantry. The relative movement of the MCS X axis would be added to both ACS axes. The two ACS axes can also be commanded independently for minor alignment adjustments.

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™