You are here: Tools > AKD into KAS > Workbench Reference > AIN.CUTOFF

AIN.CUTOFF

General Information

Type

NV Parameter

Description

Sets the analog input low-pass filter cutoff frequency.

Units

Hz

Range

0 to 10,000 Hz

Default Value

5,000 Hz

Data Type

Float

Start Version

M_01-00-00-000

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

5000h/0

M_01-00-00-000

Description

AIN.CUTOFF sets the break frequency in Hz for two cascaded single-pole low-pass filters on the hardware command input. Since the two poles are cascaded at the same frequency, the -3 dB frequency is 0.64*AIN.CUTOFF in hertz and the 10% to 90% step response rise time is 0.53/AIN.CUTOFF in seconds.

Suggested operating values are as follows:

Related Topics

Analog Input on pg. 1

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™