You are here: Tools > AKD into KAS > Workbench Reference > AIN.OVFTHRESH

AIN.OVFTHRESH

General Information

Type

NV Parameter

Description

Over voltage threshold for user defined fault on analog input.

Units

V

Range

-10 to 10

Default Value

10V

Data Type

Float

Start Version

M_01-13-09-000

Description

This parameter defines the over voltage threshold for analog input. If AIN.VALUE is larger than AIN.OVFTHRESH, and AIN.MODE = 3 (user defined fault mode), an over voltage fault is generated.

Related Topics

Analog Input on pg. 1 | AIN.MODE on pg. 1 | AIN.UVWTHRESH on pg. 1 | AIN.UVFTHRESH on pg. 1 | AIN.OVWTHRESH on pg. 1

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™