You are here: Tools > AKD into KAS > Workbench Reference > AOUT MODE

AOUT.MODE

General Information

Type

NV Parameter

Description

Sets the analog output mode.

Units

N/A

Range

0 to 11

Default Value

0

Data Type

Integer

Start Version

M_01-00-00-000

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

3470h on pg. 1/1

M_01-00-00-000

Description

AOUT.MODE sets the analog output functionality.

AOUT.MODE

Description

0

User variable. The analog output signal is determined by the user (using AOUT.VALUEU).

1

Actual velocity. The analog signal describes the current velocity value (VL.FB).

2

Velocity error. The analog signal describes the velocity error value.

3

Velocity command. The analog signal describes the velocity command value.

4

Actual current. The analog signal describes the actual current value.

5

Current command. The analog signal describes the current command value.

6

Actual position. The analog signal describes the current position value.

7

Position error. The analog signal describes the position error value.

8

Triangle wave. The analog signal is a triangle wave (sawtooth pattern).

9

Debug mode. In this mode the user can define a drive variable to monitor via the analog output (AOUT.VALUEU).

10

Unfiltered Velocity (VL.FBUNFILTERED)

11

Filtered Velocity - 10Hz Lowpass (VL.FBFILTER)

Example

You can use AOUT.MODE and AOUT.VALUEU to configure an output signal as follows:

-->AOUT.MODE 0

-->AOUT.VALUEU 5

-->AOUT.VALUEU 4.33

Related Topics

Analog Output on pg. 1

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™