You are here: Tools > AKD into KAS > Workbench Reference > BODE.EXCITEGAP

BODE.EXCITEGAP

General Information

Type

R/W Parameter

Description

Controls how often the excitation is updated.

Units

DriveControl device for regulating the speed, torque and position of a motor samples

Range

1 to 255 drive samples

Default Value

2 drive samples

Data Type

N/A

Start Version

M_01-00-00-000

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

5013h/0

M_01-00-00-000

Description

BODE.EXCITEGAP controls how often the excitation is updated. The excitation is updated every n drive samples, where n is BODE.EXCITEGAP. For example, if BODE.EXCITEGAP = 2, then the excitation is updated every 2/(16,000 Hz) = 1/8,000 Hz = 0.000125 sec. When measuring a system, update the excitation only as often as the data is recorded.

Example

Set excitation update rate to 8,000 Hz:

-->BODE.EXCITEGAP 2

Set excitation update rate to 4,000 Hz:

-->BODE.EXCITEGAP 4

Get excitation update rate (already set to 8000 Hz):

-->BODE.EXCITEGAP 2

Related Topics

Using the Performance Servo Tuner on pg. 1 | Using the Performance Servo Tuner: Advanced on pg. 1

Scope on pg. 1

Settings on pg. 1

F126 on pg. 1

Error: Invalid Bode plot mode for this function. on pg. 1

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™