You are here: Tools > AKD into KAS > Workbench Reference > CMP0.SOURCEVALUE, CMP1.SOURCEVALUE

CMPx.SOURCEVALUE

General Information

Type

R/O Parameter

Description

Reads the current value of the selected source for CMPx.SOURCE.

Units

Units depend on value of CMPx.SOURCE. See table below.

Range

N/A

Default Value

N/A

Data Type

Float

Start Version

M_01-13-00-000

Units

CMPx.SOURCE Units
0 (FB1) Depends on FB1.PUNIT on pg. 1 or custom units.
1 (FB2) Depends on FB2.PUNIT on pg. 1 or custom units.
2 (FB3) Depends on FB2.PUNIT on pg. 1 or custom units.
3 (PL.FB) Depends on UNIT.PLINEAR or UNIT.PROTARY
Rotary: counts, rad, deg, (custom units), 16-bit counts
Linear: counts, mm, µm, (custom units), 16-bit counts

Compare functionality is supported on hardware revisions D, DB, DA, and higher depending on the drive type. Check the label on the side of the drive to ensure the AKD meets one of the following requirements.

AKD Type Hardware Revision Supported
AKD Revision D or higher
PDMM Revision DB or higher
AKD-T-IC"Integrated Circuits" Miniaturized electronic circuits (consisting mainly of semiconductor devices, as well as passive components) that have been manufactured in the surface of a thin substrate of semiconductor material Revision DA or higher

Description

Reads the current value of the selected source for CMPx.SOURCE.

Example

If CMP0.SOURCE = 3 (PL.FB), CMP0.SOURCEVALUE will return the current value of PL.FB.

Related Topics

Compare Engines on pg. 1 | CMPx.SOURCEVALUE

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™