COGCOMP.RANGELOW

This content is not applicable to KAS, using either a PAC"Programmable Automation Controller" PAC is a compact controller that combines the features and capabilities of a PC-based control system with that of a typical programmable logic controller (PLC). A PAC thus provides not only the reliability of a PLC, but also the task flexibility and computing power of a PC. Additionally, because they function and communicate over popular network interface protocols, PACs are able to transfer data from the machines they control to other machines and components in a networked control system or a PDMM.

General Information

Type

NV Parameter

Description

Stores the position of the lower end of the range where cogging compensation is active on a linear axis.

Units

Position units

Range

-9,223,372,036,854,774 [counts] to 9,223,372,036,854,774 [counts] or equivalent in position units

Default Value

0

Data Type

Float

Start Version

M_01-14-06-001

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Index/Subindex Object Start Version

EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

5418h/0

M_01-14-06-001

Description

This parameter stores the position of the lower end of the range where cogging compensation is active on a linear axis.

When the value is changed while compensation values are configured, the compensation values will be redistributed over the new range, which will most likely lead to incorrect compensation.

Before starting COGCOMP.TEACH on pg. 1 on a linear axis, the value in COGCOMP.RANGELOW has to be smaller than COGCOMP.RANGEHIGH on pg. 1.

Related Topics

 

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™