DOUT1.PARAM AND DOUT2.PARAM

General Information

Type

NV Parameter

Description

Sets extra parameters for the digital output(s).

Units

N/A

Range

0

Note: Range changes based on Digital Output Mode. See below.

Default Value

0

Data Type

Integer

Start Version

M_01-00-00-000

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Index/Subindex Object Start Version

EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

3475h/1

DOUT1.PARAM

M_01-00-00-000

3475h/2

DOUT2.PARAM

Description

Set the extra parameter needed for the digital output's calculations.

Range

DOUTx.PARAM is used for various Digital Output modes. This causes the parameter’s range to change based on the current Digital Output mode selected with the corresponding DOUTx.MODE.

Below is a list of the possible range for each Digital Output Mode.

If an output mode is not listed, then the default range of 0 is used.

Input Mode Min Max Notes
3 Position Min Position Max This value changes based on user selected position units.
4 Position Min Position Max This value changes based on user selected position units.
5 Position Min Position Max This value changes based on user selected position units.
6 Position Min Position Max This value changes based on user selected position units.
12 0 Velocity Max This value changes based on user selected velocity units.
13 0 Velocity Max This value changes based on user selected velocity units.
15 0 255 None.
17 Position Min Position Max This value changes based on user selected position units.

Dependency on DOUTx.MODE

Since the default range of DOUTx.PARAM does not allow a user to enter a value, DOUTx.MODE must be set to a mode which uses DOUTx.PARAM before a value can be set.

Each time DOUTx.MODE is changed, DOUTx.PARAM is automatically set to zero to prevent unintended interactions.

Digital Output Mode 15: PLS.STATE bits OR connected

The output mode produces a high signal if at least one of the PLS.STATE bits is high (the PLS is active) and if the corresponding bit in the DOUTx.PARAM parameter also has been set to high. The DOUTx.PARAM command connects the PLS.STATE bits to the digital output itself and thus acts as an enable mask.

In mode 15 DOUTx.PARAM is set from the Digital Outputs section of the Programmable Limit Switches screen.

This mode is valid for all opmodes and command source combinations.

Example

|<- Bit 7 to 0 ->|

DOUT1.PARAM = 23 = 0b 0 0 0 1 0 1 1 1 (Binary code)

The digital output 1 is active when bit 0 or bit 1 or bit 2 or bit 4 of PLS.STATE is high. All other bits within PLS.STATE are not considered by the digital output mode due to the DOUT1.PARAM setting. Do not use decimal places for the DOUTx.PARAM parameter for this particular digital output mode.

Related Topics

Digital Outputs on pg. 1

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™