You are here: Tools > AKD into KAS > Workbench Reference > DRV.BLINKDISPLAY

DRV.BLINKDISPLAY

General Information

Type

Command

Description

Causes the display to blink for 10 seconds.

Units

N/A

Range

N/A

Default Value

N/A

Data Type

N/A

Start Version

M_01-00-00-000

*For Profinet, write a value of 0 into the PNU to execute a command.

Description

DRV.BLINKDISPLAY causes the drive display located on the front of the drive to blink for 10 seconds.

This command allows the user to identify the drive that is currently communicating with WorkBench.

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™