You are here: Tools > AKD into KAS > Workbench Reference > DRV.BOOTTIME

DRV.BOOTTIME

General Information

Type

R/O

Description

Returns the time when the current session booted up.

Units

Days:Hours:Minutes:Seconds

Range

N/A

Default Value

N/A

Data Type

String

Start Version

M_01-06-05-000

Description

DRV.BOOTTIME returns the time that the current session started running.This time includes total amount of time from all previous sessions.

This keyword can be used with DRV.RUNTIME to determine the length of time the drive has been running since it was last power cycled.

Session Time = DRV.RUNTIME – DRV.BOOTTIME

Related Topics

DRV.RUNTIME on pg. 1

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™