You are here: Tools > AKD into KAS > Workbench Reference > DRV.CMDSOURCE

DRV.CMDSOURCE

General Information

Type

NV Parameter

Description

Sets the command source (service, fieldbus, analog input, gearing, digital, or Bode).

Units

N/A

Range

0 to 5

Default Value

0

Data Type

Integer

Start Version

M_01-00-00-000

Description

DRV.CMDSOURCE specifies the source of the command to the drive. DRV.OPMODE on pg. 1 sets the operation mode to the relevant control loop.

DRV.CMDSOURCE values can be set as follows:

Value

Description

0

Service, TCP/IP command

1

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design command

2

Gearing command

3

Analog command

5 Program command

If DRV.CMDSOURCE is set to 5 then DRV.OPMODE must be set to 3.

DRV.CMDSOURCE can be changed while the drive is enabled or disabled. If you use the terminal to change the operation mode, then it is recommended that you disable the drive before changing the command source.

Example

To set the command source to the TCP/IP channel and the operation mode to velocity:

-->DRV.CMDSOURCE 0

-->DRV.OPMODE 1

Related Topics

DRV.OPMODE on pg. 1

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™