You are here: Tools > AKD into KAS > Workbench Reference > DRV.CUSTOMIDENTIFIER

DRV.CUSTOMIDENTIFIER

General Information

Type

NV Parameter

Description

Sets the customer defined identifier string for a device.

Units

N/A

Range

N/A

Default Value

N/A

Data Type

String

Start Version

M_01-12-05-000

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Index/Subindex Object Start Version

EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

2032h/0

M_01-12-05-000

Description

Use DRV.CUSTOMIDENTIFIER to assign a unique string to a device. The string must use the following formatting rules:

The string is displayed on the device overview screen and in the start page's device discovery table.

Related Topics

DRV.NAME on pg. 1

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™