You are here: Tools > AKD into KAS > Workbench Reference > DRV.DBILIMIT

DRV.DBILIMIT

General Information

Type

NV Parameter

Description

Sets the maximum amplitude of the current for dynamic braking.

Units

Arms

Range

0 to minimum of drive peak currentThe effective value of the peak current (DRV.IPEAK) and motor peak current (MOTOR.IPEAK).

Default Value

Minimum of drive continuous current (DRV.ICONT) and motor continuous current (MOTOR.ICONT).

Data Type

Float

Start Version

M_01-00-00-000

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

3444h/0

M_01-00-00-000

Description

This parameter sets the maximum amplitude of the current for dynamic braking.

Example

Setting DRV.DBILIMIT to 2 limits the dynamic brake current to 2 Arms.

Related Topics

Controlled Stop

CS Parameters

Dynamic Braking

DRV.DISMODE on pg. 1

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™