You are here: Tools > AKD into KAS > Workbench Reference > DRV.DISSOURCESMASK

DRV.DISSOURCESMASK

General Information

Type

R/O parameter

Description

Returns a bitmap of all bits in DRV.DISSOURCES that can be set to one on a given drive.

Units

N/A

Range

N/A

Default Value

N/A

Data Type

Integer

Start Version

M_01-07-00-000

Description

DRV.DISSOURCESMASK is a bitwise parameter that returns all possible causes of a drive disable. If a bit is set, the drive can be disabled for this reason.

The return value specific bits are as follows:

Bit Status and Response
0 Software triggered disable
1 Fault exists
2 Hardware EnableEnable signal for the drive, Hardware-Enable with 24V signal to X8, Software-Enable command by setup Software, fieldbus or permanently set. Both are required for enabling the drive. input inactive
3 In-rush relay state prevents enable
4 Initialization not complete
5 Controlled stop requested from digital input
6 Field bus requested disable

For most AKD models, this parameter will return the value 63.

Related Topics

DRV.DISSOURCES on pg. 1

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™