|
General Information |
|
|---|---|
|
Type |
R/W Parameter |
|
Description |
|
|
Units |
ms |
|
Range |
0 to 120,000 ms |
|
Default Value |
1,000 ms |
|
Data Type |
U32 |
|
Start Version |
M_01-00-00-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
3445h/0 |
M_01-00-00-000 |
Description
This timer starts when DRV.DIS on pg. 1 is issued (regardless of the DRV.DIS on pg. 1 origin). After this timeout elapses, the actual state of the drive is compared to the DRV.DISMODE on pg. 1 setting. If the actual state does not match the DRV.DISMODE on pg. 1 setting, a fault is reported and the hardware immediately executes the DRV.DISMODE setting (for instance, disable or activate dynamic brake). Setting DRV.DISTO to 0 will disable the timeout.
Related Topics
DRV.DIS on pg. 1, DRV.DISMODE on pg. 1
|
Copyright © 2015 Kollmorgen™ |
|