|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
3493h/0 |
M_01-00-00-000 |
Description
This parameter sets the direction of the emulated encoder output (EEO). DRV.DIR on pg. 1 also effects the output direction (through an XOR, "exclusive or", operation). The drive uses DRV.DIR on pg. 1 and DRV.EMUEDIR to decide the direction of the EEO. If DRV.DIR on pg. 1 and DRV.EMUEDIR have the same value, then DRV.EMUEDIR is set to 0 (meaning an increase in the motor feedback will result an increase of the EEO and vice-versa). If these parameters have different values, then DRV.EMUEDIR is set to 1 (meaning an increase in the motor feedback will result in a decrease of the EEO and vice-versa).
|
Copyright © 2015 Kollmorgen™ |
|