You are here: Tools > AKD into KAS > Workbench Reference > DRV.EMUEPULSEWIDTH

DRV.EMUEPULSEWIDTH

General Information

Type

TBD

Description

Sets the encoder output pulse width for modes 6 to 7.

Units

us(microseconds)

Range

4.08 us to 2621.48 us

Default Value

4.08 us

Data Type

Float

Start Version

M_01-00-00-000

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

520Dh/0

M_01-00-00-000

Description

EMU Encoder Out PulseWhen the step gets activated, the action is activated for a single execution, and possibly once again when the step is deactivated Width Register

Sets pulse width for CW/CCW and Step and Direction modes. This parameter does not effect the A quad B mode. To calculate emuOutPulseWidth:

(Desired pulse width -40 nsec)/520 nsec

Requirement DSFPGA-03-306
Bits Bits Description
11:0 emuOutPulseWidth Read/Write
12 bit unsigned number minimum resolution is 520 nsec.
ResetNew start of the microprocessor state – 0
15:12   reserved

Example

50 usecs pulse width

emuOutPulseWidth = (50 usecs – 40 nsec)/520 nsec = 96

actual pulse = 96*520 nsec + 40 nsec = 49.88 usecs.

Related Topics

DRV.EMUEMODE on pg. 1

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™