You are here: Tools > AKD into KAS > Workbench Reference > DRV.FAULTHIST

DRV.FAULTHIST

General Information

Type

R/O Parameter

Description

Reads the last 50 faults from NV memory.

Units

N/A

Range

N/A

Default Value

N/A

Data Type

N/A

Start Version

M_01-00-00-000

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

2012h

2013h

M_01-00-00-000

Description

DRV.FAULTHIST returns the last 50 faults that occurred in the drive. The faults are shown with their fault number (which matches the one displayed on the drive display) and a time stamp that indicates when they last occurred.

Issue a DRV.CLRFAULTHIST on pg. 1 to clear this fault log.

Related Topics

DRV.FAULTS on pg. 1, DRV.CLRFAULTHIST on pg. 1

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™