|
General Information |
|
|---|---|
|
Type |
R/O Parameter |
|
Description |
|
|
Units |
1/4,294,967,296 rev |
|
Range |
0 to 4,294,967,295 rev |
|
Default Value |
0 rev |
|
Data Type |
Integer |
|
See Also |
|
|
Start Version End Version |
M_01-00-00-000 M_01-03-00-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
2050h/0 |
M_01-00-00-000 |
Description
When the EEO is selected as an input (DRV.EMUEMODE on pg. 1=3,4,5), this parameter reads the EEO value (where 4,294,967,296 is a full revolution, then the value rolls over). DRV.EMUERES on pg. 1 defines the how many counts constitute a revolution on the EEO. This parameter represents the feedback 2 positions when feedback 2 is configured to be active.
When secondary feedback is selected (DRV.EMUEMODE is 0 and FB2.SOURCE = 1 (X9), or FB2.SOURCE = 2 (X7)), this parameter represents the secondary feedback position (where 4,294,967,296 is a full revolution, then the value rolls over). FB2.ENCRES defines how many counts define a revolution for the secondary feedback.
Related Topics
|
Copyright © 2015 Kollmorgen™ |
|