You are here: Tools > AKD into KAS > Workbench Reference > DRV.HANDWHEELSRC

DRV.HANDWHEELSRC

General Information

Type

NV Parameter

Description

Selects the feedback for handwheel operation.

Units

None

Range

2-3

Default Value

2

Data Type

U8

Start Version

M_01-05-08-000

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

5263h/0

M_01-05-08-000

Description

This command sets the feedback which will be used as the handwheel source. If the selected Feedback is incompatible with the selected emulated encoder mode, a warning will be displayed.

Feedback 3 is only supported on drives with model numbers similar to AKD-x-xxxxx-NBxx-xxxx and will only work with Endat 2.2 multiturn encoder.

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™