|
General Information |
|
|---|---|
|
Type |
R/O |
|
Description |
Status of the hardware enable. |
|
Units |
N/A |
|
Range |
0 to 1 |
|
Default Value |
N/A |
|
Data Type |
Integer |
|
Start Version |
tbd |
Description
Status of the Hardware EnableEnable signal for the drive, Hardware-Enable with 24V signal to X8, Software-Enable command by setup Software, fieldbus or permanently set. Both are required for enabling the drive..
0 - not enabled
1 - enabled
Notes: This parameter reflects the status of the hardware enable only, not if the status of the power stage. The status of the power stage enable is determined by DRV.ACTIVE.
Related Topics
DRV.DISSOURCES on pg. 1 | DRV.ACTIVE
|
Copyright © 2015 Kollmorgen™ |
|