You are here: Tools > AKD into KAS > Workbench Reference > DRV.IPEAK

DRV.IPEAK

General Information

Type

R/O Parameter

Description

Reads the peak rated current value.

Units

Arms

Range

N/A

Default Value

N/A

Data Type

Float

Start Version

M_01-00-00-000

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

5084h/0

M_01-00-00-000

Description

DRV.IPEAK returns the drive peak rated current in Arms.

Related Topics

Foldback

DRV.ICONT on pg. 1

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™