You are here: Tools > AKD into KAS > Workbench Reference > DRV.LIST

DRV.LIST

General Information

Type

R/O Parameter

Description

Reads the list of available parameters and commands.

Units

N/A

Range

N/A

Default Value

N/A

Data Type

String

Start Version

M_01-00-00-000

Description

DRV.LIST reads the list of available commands and parameters from the drive.

To filter this list, enter DRV.LIST followed by the prefix of the commands and parameters that you wish to display.

Example

Return a list of all available commands in the system:

-->DRV.LIST

Return all commands with the prefix DRV:

-->DRV.LIST DRV

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™