|
General Information |
|
|---|---|
|
Type |
R/W Parameter |
|
Description |
|
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
N/A |
|
Start Version |
M_01-00-00-000 |
Description
DRV.MEMDATA reads or writes a value using the address set by DRV.MEMADDR on pg. 1 . The write value accepts decimal or "0x" hexadecimal format. The read value defaults to decimal display but can be set to hexadecimal with the command "DRV.READFORMAT on pg. 1 16".
Examples
Read a value from internal address:
-->DRV.MEMADDR 0x1234.u32
--DRV.MEMDATA
3800219712
Write a decimal value to an internal address:
-->DRV.MEMDATA 123
Write a hexadecimal value to an internal address:
-->DRV.MEMDATA 0xFEDC
|
Copyright © 2015 Kollmorgen™ |
|