|
General Information |
|
|---|---|
|
Type |
R/O Parameter |
|
Description |
|
|
Units |
N/A |
|
Range |
0 to 4,294,967,295 |
|
Default Value |
N/A |
|
Data Type |
Integer |
|
See Also |
N/A |
|
Start Version |
M_01-00-00-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
3492h/0 |
M_01-00-00-000 |
Description
This command indicates the current status of the drive internal motion (see table below).
|
Bit |
Significance |
Description |
|---|---|---|
|
0 |
0x00000001 |
Motion task is active (high active) |
|
1 |
0x00000002 |
Home position found /reference point set (high active) |
|
2 |
0x00000004 |
Home routine finished (high active). Bits 1 and 2 both must be set to confirm that the homing process is complete. |
|
3 |
0x00000008 |
HomingThe Homing procedure allows, based on a position measurement, to set a position offset to the motor in order to ensure it is physically at the home position active (high active) |
|
4 |
0x00000010 |
Homing error condition has occurred (high active)* |
|
5 |
0x00000020 |
Slave in electronic gearing mode synchronized (high active) |
|
6 |
0x00000040 |
Electronic gearing is active (high active) |
|
7 |
0x00000080 |
Emergency stop procedure in progress (high active) |
|
8 |
0x00000100 |
Emergency stop procedure has an error (high active) |
|
9 |
0x00000200 |
Service motion active (high active) |
|
10 |
0x00000400 |
A motion task could not be activated /invalid MT (high active)** |
|
11 |
0x00000800 |
Motion task target position has been reached. See also (high active). |
|
12 |
0x00001000 |
Motion task target velocity has been reached. See also (high active). |
|
13 |
0x00002000
|
Motion task encountered an exception. A motion task exception can happen during a static motion task activation, or during activation of motion task on the fly (when velocity is not zero). The status bit will be reset automatically on successful activation of any motion, or by a command DRV.CLRFAULT. |
|
14 |
0x00004000 |
The target position of a motion task has been crossed. This situation occurs for motion tasks with a change on the fly when triggering the DRV.STOP on pg. 1 command just before the reaching the target velocity of the current active motion task. The ramp-down procedure with the motion task deceleration ramp causes the target position to be crossed (high active). |
* A possible error condition for homing to a reference switch could be that no reference switch was found between two hardware limit switches.
** A possible error condition for an invalid motion task could be that a motion task tried to trigger automatically following motion task that has never been initialized (called an "empty motion" task).
|
Copyright © 2015 Kollmorgen™ |
|