You are here: Tools > AKD into KAS > Workbench Reference > DRV.REBOOT

DRV.REBOOT

General Information

Type

Command

Description

Performs a software reboot.

Units

N/A

Range

N/A

Default Value

N/A

Data Type

Integer

Start Version

M_01-13-08-000

Description

This parameter performs a software reboot when the following command is issued in the WorkBench terminal:

DRV.REBOOT 0xAABBCCDD

WorkBench will disconnect from the AKD when the reboot command is executed. The AKD can be reconnected to WorkBench approximately one minute after the reboot command is issued. The parameters stored in non-volatile memory will be restored to the AKD once rebooted.

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™