You are here: Tools > AKD into KAS > Workbench Reference > DRV.RSTVAR

DRV.RSTVAR

General Information

Type

Command

Description

Sets default values in the drive without re-booting the drive and without resetting the NV memory.

Units

N/A

Range

N/A

Default Value

N/A

Data Type

N/A

Start Version

M_01-00-00-000

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

Communication SDOs on pg. 1/1

M_01-00-00-000

*For Profinet, write a value of 0 into the PNU to execute a command.

Description

DRV.RSTVAR causes the drive to return to the default values without the need to re-boot the drive first and without resetting the NV memory. Use DRV.RSTVAR to return to the default settings and recover a working drive.

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™