|
General Information |
|
|---|---|
|
Type |
R/O Parameter |
|
Description |
|
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
String |
|
Start Version |
M_01-00-00-000 |
Description
DRV.VERIMAGE reads the versions of the different images in the drive. This parameter returns the version data from each image .i00 file.
Example
Below is an example of the output for this parameter:
Danaher Motion - Digital Servo DriveA servo drive is a special electric amplifier used to power electric servo motors. It monitors feedback signals from the motor and continually adjusts for deviation from expected behavior
------------------------------------
Resident Firmware: R_0-0-11
Operational Firmware: M_0-0-15
Resident FPGA"Field-Programmable Gate Array" FPGA is a semiconductor device that can be configured by the customer or designer after manufacturing; hence the name "field-programmable": FPB004_0001_00_07
Operational FPGA : FP0004_0001_00_07
|
Copyright © 2015 Kollmorgen™ |
|