|
General Information |
|
|---|---|
|
Type |
R/O Parameter |
|
Description |
|
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
N/A |
|
See Also |
FBUS.PARAM1 TO FBUS.PARAM10 on pg. 1, FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design documentation |
|
Start Version |
M_01-02-00-000 |
Description
FBUS.PLLSTATE returns the status of the phase locked loop (PLL). The PLL states are as follows:
| PLL State | Description |
|---|---|
|
PLL not activated |
This state is set using FBUS.PARAM02. Not each fieldbus or operation mode needs synchronization. |
|
PLL activated, but unlocked |
The PLL is activated but has not yet been locked successfully. This state is related to the fieldbus master, as well as to the fieldbus mode of operation. |
|
PLL activated and locked |
PLL is fully operational and locked |
|
Copyright © 2015 Kollmorgen™ |
|