You are here: Tools > AKD into KAS > Workbench Reference > FBUS.REMOTE

FBUS.REMOTE

General Information

Type

R/W Parameter

Description

Changes or shows the control of the drive (fieldbus master/telnet)

Units

N/A

Range

0 to 1

Default Value

0

Data Type

U8

Start Version

M_01-05-06-000

Description

DS402 (CAN"Controller area network" CAN is a broadcast, differential serial bus standard developed for connecting electronic control units. Each node is able to send and receive messages, but not simultaneously/EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs):

With this parameter the bit 9 (remote) of the DS402-status word can be set directly via Telnet to show the DS402-master-system that the control is removed. The master has to react on that.

Related Topics

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Manuals

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™