You are here: Tools > AKD into KAS > Workbench Reference > FBUS.SAMPLEPERIOD

FBUS.SAMPLEPERIOD

General Information

Type

NV Parameter

Description

Sets fieldbus sample period.

Units

Whole multiples of MTS 250 µs

Range

4 to 128 and value must be a multiple of 4

Default Value

32 = 2 ms

Data Type

U8

See Also

Appendix B: FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Manuals

Start Version

M_01-00-00-000

Fieldbus

Index/Subindex

Object Start Version

EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

Profile specific SDOs/0

M_01-00-00-000

Description

This parameter sets the fieldbus cycle time. It is normally written in the startup phase of the field busses via the object 60C2 subindex 1 (interpolation time units) and 2 (interpolation time index), where the index stands for a power of 10 seconds (for instance, -3 stands for milliseconds) and the units are the counts of these units. Kollmorgen recommends the following standard cycle rates, 250 us (4), 500 us (8), 1 ms (16), 2 ms (32), 4 ms (64).

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™