You are here: Tools > AKD into KAS > Workbench Reference > FBUS.STATE

FBUS.STATE

General Information

Type

R/O

Description

Reads the state of the fieldbus.

Units

N/A 

Range

Depends on fieldbus. See table below.

Default Value

Depends on fieldbus. See table below.

Data Type

Integer

Start Version

M_01-08-00-000

Description

FBUS.STATE returns the current state of the fieldbus. The value returned is dependent upon the fieldbus being used.

Value CANopen over CAN"Controller area network" CAN is a broadcast, differential serial bus standard developed for connecting electronic control units. Each node is able to send and receive messages, but not simultaneously CANopen over EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs
-1 Not connected Not connected
0 Init. -
1 N/A Init.
2 N/A Pre-operational
3 - Boot
4 Stopped Safe-operational
5 Operational -
8 - Operational
127 Pre-operational -

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™