You are here: Tools > AKD into KAS > Workbench Reference > FBUS.SYNCACT

FBUS.SYNCACT

General Information

Type

R/O Parameter

Description

Reads actual distance from the desired sync distance.

Units

ns

Range

0 to 250,000 ns

Default Value

0 ns

Data Type

Integer, U 32

See Also

Appendix B: FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Manuals

Start Version

M_01-00-00-000

Fieldbus

Index/Subindex

Object Start Version

EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

3496h/2

M_01-00-00-000

Description

This parameter reads actual distance from the desired sync distance.

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™