You are here: Tools > AKD into KAS > Workbench Reference > FBUS.SYNCDIST

FBUS.SYNCDIST

General Information

Type

NV Parameter

Description

Sets time target for synchronization.

Units

ns

Range

0 to 2,500,000 ns

Default Value

100,000 ns

Data Type

Integer, U32

See Also

Appendix B: FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Manuals

Start Version

M_01-00-00-000

Fieldbus

Index/Subindex

Object Start Version

EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

3496h/1

M_01-00-00-000

Description

This parameter sets time target for synchronization.

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™