You are here: Tools > AKD into KAS > Workbench Reference > HWLS.POSSTATE

HWLS.POSSTATE

General Information

Type

R/O Parameter

Description

Reads the status of the positive hardware limit switch.

Units

N/A

Range

0 to 1

Default Value

N/A

Data Type

Integer

See Also

HWLS.NEGSTATE on pg. 1

Start Version

M_01-00-00-000

Description

HWLS.POSSTATE reads the status of the positive hardware limit switch as follows:

0 = Low

1 = High

Related Topics

 

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™