IL.DFOLDT

General Information

Type

R/W Parameter

Description

Reads the drive foldback time constant of the exponential current drop (foldback).

Units

s

Range

1 to 65.535 s

Default Value

Usually 2.500 s, but may change according to the drive type.

Data Type

Float

See Also

Foldback

Start Version

M_01-00-00-000

Description

IL"Instruction list" This is a low-level language and resembles assembly.DFOLDT is the time constant of the exponential drop (foldback) of the current towards the drive continuous current.

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™