|
General Information |
|
|---|---|
|
Type |
R/O Parameter |
|
Description |
Reads the sigma-delta measured current in the u-winding of the motor. |
|
Units |
A |
|
Range |
± DriveControl device for regulating the speed, torque and position of a motor peak currentThe effective value of the peak current (DRV.IPEAK) |
|
Default Value |
N/A |
|
Data Type |
Float |
|
See Also |
N/A |
|
Start Version |
M_01-00-00-000 |
Description
This parameter displays the measured current in the u-winding of the motor.
Related Topics
|
Copyright © 2015 Kollmorgen™ |
|