You are here: Tools > AKD into KAS > Workbench Reference > IL.IVFB

IL.IVFB

General Information

Type

R/O Parameter

Description

Sets the sigma-delta measured current in the u-winding of the motor.

Units

A

Range

± DriveControl device for regulating the speed, torque and position of a motor peak currentThe effective value of the peak current (DRV.IPEAK)

Default Value

0 A

Data Type

Float

See Also

N/A

Start Version

M_01-00-00-000

Description

IL"Instruction list" This is a low-level language and resembles assembly.IVFB is an offset value that is added to the measured current in the u-winding of the motor. This value is used for compensating for an error in the current measurement. The drive measures 256 times the current in the u-winding when powering-up the drive. Afterwards, the drive calculates the average value of the measured current and uses this value for the offset value.

Related Topics

Current Loop on pg. 1

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™