You are here: Tools > AKD into KAS > Workbench Reference > IL.MFOLDD

IL.MFOLDD

General Information

Type

R/O Parameter

Description

Sets the motor foldback maximum time at motor peak currentThe effective value of the peak current.

Units

s

Range

0.1 to 2400 s

Default Value

10 s

Data Type

Float

See Also

Foldback

Start Version

M_01-00-00-000

Description

IL"Instruction list" This is a low-level language and resembles assembly.MFOLDD sets the maximum time allowed for the motor to remain at peak current before starting to fold towards the motor continuous current. When at motor peak current, IL.MFOLDD is the amount of time before the foldback algorithm starts to reduce the current.

Related Topics

Current Loop on pg. 1

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™