You are here: Tools > AKD into KAS > Workbench Reference > IL.MFOLDR

IL.MFOLDR

General Information

Type

R/O Parameter

Description

Sets the motor foldback recovery time.

Units

s

Range

0.1 to 65,535 s

Default Value

Calculated from other foldback parameters.

Data Type

Float

See Also

Foldback

Start Version

M_01-00-00-000

Description

IL"Instruction list" This is a low-level language and resembles assembly.MFOLDR sets the recovery time for the motor foldback algorithm. If 0 current is applied for at least the recovery time duration, it is possible to apply motor peak currentThe effective value of the peak current for the duration of IL.MFOLDD time.

The IL.MFOLDR value is automatically calculated from other foldback parameters.

Related Topics

Current Loop on pg. 1

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™