You are here: Tools > AKD into KAS > Workbench Reference > IL.MFOLDT

IL.MFOLDT

General Information

Type

R/O Parameter

Description

Sets the motor foldback time constant of the exponential current drop (foldback).

Units

s

Range

0.1 to 2,400 s

Default Value

10 s

Data Type

Float

See Also

Foldback

Start Version

M_01-00-00-000

Description

IL"Instruction list" This is a low-level language and resembles assembly.MFOLDT sets the time constant of the exponential drop (foldback) of the current towards motor continuous current.

Related Topics

Current Loop on pg. 1

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™