You are here: Tools > AKD into KAS > Workbench Reference > IL.MIMODE

IL.MIMODE

General Information

Type

NV parameter

Description

Motor protection mode.

Units

N/A

Range

0 to 1

Default Value

0

Data Type

Integer

See Also

IL.MI2T on pg. 1,  IL.MI2TWTHRESH on pg. 1

Start Version

M_01-04-01-000

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

3427h/1

M_01-00-00-000

Description

This parameter determines the method of the motor protection.

0 – The motor foldback mechanism is responsible for protecting the motor from overload.

1 – The Motor I2t algorithm is responsible for protecting the motor from overload.

Related Topics

Foldback on pg. 1

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™