You are here: Tools > AKD into KAS > Workbench Reference > IL.VCMD

IL.VCMD

General Information

Type

R/O Parameter

Description

Reads the output of the q-component PI regulator.

Units

Vrmsrms stands for root mean square (also known as the quadratic mean)

Range

0 Vrms to bus voltage

Default Value

N/A

Data Type

Integer

Start Version

M_01-00-00-000

Description

Reads the output of the current loop that controls the q-component of the current.

Related Topics

Current Loop on pg. 1

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™