|
General Information |
|
|---|---|
|
Type |
Command |
|
Description |
|
|
Units |
N/A |
|
Range |
0 to 2 |
|
Default Value |
0 |
|
Data Type |
Integer |
|
See Also |
N/A |
|
Start Version |
M_01-00-00-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
M_01-07-04-000 |
Description
This command allows a user to release or apply the motor brake.
0 = DriveControl device for regulating the speed, torque and position of a motor controls the brake.
1 = Brake is released.
2 = Brake is applied.
A digital input mode can also be used for the same purpose. The two mechanisms are independent.
Related Topics
|
Copyright © 2015 Kollmorgen™ |
|