|
General Information |
|
|---|---|
|
Type |
R/O Parameter |
|
Description |
|
|
Units |
N/A |
|
Range |
Brake released or not present. Brake applied. |
|
Default Value |
Brake applied or not present. |
|
Data Type |
String |
|
See Also |
N/A |
|
Start Version |
M_01-00-00-000 |
Description
This parameter reads the actual status of the motor brake and can only show two states:
1 = Brake released or not present
2 = Brake applied
Related Topics
|
Copyright © 2015 Kollmorgen™ |
|