|
General Information |
|
|---|---|
|
Type |
NV Parameter |
|
Description |
|
|
Units |
Vpeak/krpm for Rotary Motors Vpeak/m/s for Linear Motors |
|
Range |
0.0 to 100,000 |
|
Default Value |
0 |
|
Data Type |
Float |
|
See Also |
N/A |
|
Start Version |
M_01-03-06-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
5260h/0 |
M_01-03-06-000 |
Description
MOTOR.KE defines the back EMF constant for the motor. The back EMF constant defines how much voltage is generated at the motors coils. The relationship between MOTOR.KE and speed is described by the following equation:
Coil Voltage = MOTOR.KE * VL.FB
VL.FB is in units of krpm for rotary motors and in units of m/s for linear motors.
The maximum speed for interior permanent magnet motors (IPM) is determined by MOTOR.KE and VBUS.VALUE. An overspeed fault is generated if MOTOR.TYPE is set to 6 (IPM) and VL.FB * MOTOR.KE exceeds VBUS.VALUE.
This parameter is automatically configured for Kollmorgen motors when MOTOR.AUTOSET=1.
Related Topics
Motor on pg. 1 | VL.FB on pg. 1 | VBUS.VALUE on pg. 1
|
Copyright © 2015 Kollmorgen™ |
|