You are here: Tools > AKD into KAS > Workbench Reference > MOTOR.LQLL

MOTOR.LQLL

General Information

Type

NV Parameter

Description

Sets the line-to-line motor Lq.

Units

mH

Range

1 to 232 mH

Default Value

17.000 mH

Data Type

Float

See Also

N/A

Start Version

M_01-00-00-000

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

3455h/0

M_01-00-00-000

Description

This parameter is used to configure the motor line-to-line inductance.

Related Topics

Motor

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™